earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Explicación de procesos

Explicación de procesos


Productos AS-C, AS-B, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Funcionalidades: Funcionalidad básica
Versión del producto: 1.9
14/12/2016

Mass Renaming Objects Using Copy and Paste 

You mass rename objects using copy and paste to copy the names from, for example, a spreadsheet.

Mostrar más
action_close

In WorkStation, you can mass rename all objects that are possible to move. For example, you can rename alarms but not properties.

You can rename the objects one by one. You can also copy row-separated text from a file, such as an MS Excel file, and paste it to rename several rows in one single operation. When you paste, the copied text is pasted from the row you have clicked and down in the list. If the copied text is longer than the number of rows, pasting stops at the last row.

When you hover over the names in the Name column, the full path of the object is displayed.

To mass rename objects using copy and paste
  1. In WorkStation, select the container for the objects you want to rename or perform a search.

  2. In the List View or Search View , select the objects you want to rename.

     
    action_zoom_plus_stroke
  3. On the Edit menu, click Rename .

     
    action_zoom_plus_stroke
  4. Click the row in the Name column from which you want to start replacing the names.

  5. Copy any row-separated text, for example, from MS Excel.

  6. Press Ctrl + v .

  7. Click OK .

  • Mass Rename
  • Vista de listas
  • Search View
  • Mass Renaming Objects 
  • Moving Objects