earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos AD v2
Funcionalidades: Hardware
Versión del producto: 3.3, 2022, 2023, 2024
17/12/2021

AD v2 Communication and Power

AD v2 uses a wired (USB) connection to communicate with EcoStruxure BMS servers. During installation and commissioning, you can use a wireless access point to establish communication between AD v2 and EcoStruxure BMS servers. AD v2 can be powered either by a AS-P server, AS-B server, or USB power adapter.

Communication over a USB Connection

The preinstalled AD-Link application enables AD v2 to communicate with EcoStruxure BMS servers over a USB connection.

When AD v2 is connected to a AS-P server or AS-B server, AD v2 can be powered by the automation server through the USB cable. The screen must not be turned on constantly because this may drain the battery.

Aviso

LOSS OF DATA OR POWER

  • Use only USB cables ordered from Schneider Electric.

  • Use only USB cables that are designed for AD.

  • Do not use USB cables that exceed 3 m (10 ft).

Failure to follow these instructions can result in loss of data or power.

 
action_zoom_plus_stroke USB connection to a AS-P server or AS-B server
Figura: USB connection to a AS-P server or AS-B server
  • AD v2
  • Hardware Overview
  • Connecting an Advanced Display to an AS-P server or AS-B server
  • Connecting Advanced Display to a Power Adapter