earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: WorkStation, Project Configuration Tool
功能: 基本功能, 工程
产品版本: 2024, 7.0
2024/12/2

Timed Force Analog Object Properties – Basic Tab

Use the Basic tab to configure and view the basic properties of the Timed Force Analog object.

 
action_zoom_plus_stroke Timed Force Analog Object properties – basic tab
图: Timed Force Analog Object properties – basic tab

表格: Basic Tab

Component

Description

Value 

Displays the value of the object's output.

Force type select

Select the type of force time.

Force duration

Select the duration of the force in minutes.

Force until

Select the date and time at which the force must end.

Input

Displays the constant or reference value of the input. 

  • Timed Force Analog Object
  • General Information Properties – Basic Tab
  • References Tab
  • Create Object Dialog – Naming the Object Page
  • Timed Force Analog Object Properties – Parameters Tab