earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos WorkStation, Project Configuration Tool
Funcionalidades: Funcionalidad básica, Ingeniería
Versión del producto: 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024
14/12/2016

Timed Force Analog Object

The Timed Force Analog object has a single analog input that can be bound to another object to receive a value. The input's value is passed directly to a single analog output, which can be bound to an object that is to be controlled. An active timed force can be changed or cancelled as needed.

As with other Timed Force objects, the end time of the force can be configured as either a time duration or an end date and time.

  • Timed Force Objects
  • Timed Force Analog Object Properties – Basic Tab
  • Timed Force Analog Object Properties – Parameters Tab
  • Configuring a Timed Force Object for Force Until
  • Configuring a Timed Force Object for Force Duration