earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: WorkStation, Project Configuration Tool
功能: 基本功能, 工程
产品版本: 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2016/12/14

Timed Force Analog Object

The Timed Force Analog object has a single analog input that can be bound to another object to receive a value. The input's value is passed directly to a single analog output, which can be bound to an object that is to be controlled. An active timed force can be changed or cancelled as needed.

As with other Timed Force objects, the end time of the force can be configured as either a time duration or an end date and time.

  • Timed Force Objects
  • Timed Force Analog Object Properties – Basic Tab
  • Timed Force Analog Object Properties – Parameters Tab
  • Configuring a Timed Force Object for Force Until
  • Configuring a Timed Force Object for Force Duration