earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Пользовательский интерфейс

Пользовательский интерфейс


Продукты: WorkStation, Project Configuration Tool
Функции: Базовые функции, Разработка
Версия продукта: 2024, 7.0
02.12.2024

Timed Force Digital Object Properties – Basic Tab

Use the Basic tab to configure and view the basic properties of the Timed Force Digital object.

 
action_zoom_plus_stroke Timed Force Digital object properties – basic tab
Рисунок: Timed Force Digital object properties – basic tab

Таблица: Basic Tab

Component

Description

Value 

Displays the value of the object's output.

Force type select

Select the type of force time.

Force duration

Select the duration of the force in minutes.

Force until

Select the date and time at which the force must end.

Input

Displays the constant or reference value of the input. 

  • Timed Force Digital Object
  • General Information Properties – Basic Tab
  • References Tab
  • Create Object Dialog – Naming the Object Page
  • Timed Force Digital Object Properties – Parameters Tab