earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface de utilizador

Interface de utilizador


Produtos: WorkStation, Project Configuration Tool
Funcionalidades: Funcionalidade básica, Engenharia
Versão do produto: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024
24-10-2018

Timed Force Multistate Object Properties – Basic Tab

Use the Basic tab to configure and view the basic properties of the Timed Force Multistate object.

 
action_zoom_plus_stroke Timed Force Multistate object properties – basic tab
Imagem: Timed Force Multistate object properties – basic tab

Tabela: Basic Tab

Component

Description

Value 

Displays the value of the object's output.

Force type select

Select the type of force time.

Force duration

Select the duration of the force in minutes.

Force until

Select the date and time at which the force must end.

Input

Displays the constant or reference value of the input. 

  • Timed Force Multistate Object
  • General Information Properties – Basic Tab
  • References Tab
  • Create Object Dialog – Naming the Object Page
  • Timed Force Multistate Object Properties – Parameters Tab