earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: WorkStation, Project Configuration Tool
功能: 基本功能, 工程
产品版本: 2024, 7.0
2024/12/2

Timed Force Multistate Object Properties – Parameters Tab

Use the Parameters tab to view and edit the properties of the Timed Force Multistate object.

 
action_zoom_plus_stroke Timed Force Multistate object properties – parameters tab
图: Timed Force Multistate object properties – parameters tab

表格: Parameters Tab

Component

Description

Update time 

Select the frequency at which the input value is sent to the output. This value also establishes the frequency at which the force is evaluated for ending.

Transfer rate

Select the frequency at which the input is updated from other objects or devices.

  • Timed Force Multistate Object
  • General Information Properties – Basic Tab
  • References Tab
  • Create Object Dialog – Naming the Object Page
  • Timed Force Multistate Object Properties – Basic Tab