earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Explicación de procesos

Explicación de procesos


Productos AS-L, AS-B, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Funcionalidades: Alarmas, Funcionalidad básica
Versión del producto: 1.9, 2.0, 2.1, 3.0, 3.1
18/01/2018

Adding and Removing Columns

You temporarily add or remove columns in a pane or View to get a better overview of the properties.

Mostrar más
action_close

The Building Operation database is based on objects. Some objects are created when the database in installed, others are created by the engineer. Depending on the object type and your permission, you can configure objects in a many different way.

Objects that are relevant for the user are presented in the System Tree pane and in the List View. To ease recognition of objects, every object type is represented by an icon.

Content Types

Content types are predefined layouts that you save to reuse for specific types of folders or container objects.

Para obtener más información, consulte Content Types .

List View Features

You use the List View to view, manage, and mass edit objects in the Building Operation system.

Para obtener más información, consulte List View Features .

To add and remove columns
  1. In WorkStation, in the pane or View, right-click the column heading and then click Add/remove columns .

  2. In the Add/Remove dialog box, select the columns you want to add or clear the columns you want to remove.

  3. Click OK .

When you log out from WorkStation, the pane or View returns to the default columns.

  • Building Operation Objects
  • Vista de listas
  • Add/Remove Columns Dialog Box (List View)