earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Comment faire pour

Comment faire pour


Produits : AS-L, AS-B, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Fonctionnalités : Alarmes, Fonctionnalité de base
Version produit : 1.9, 2.0, 2.1, 3.0, 3.1
18/01/2018

Adding and Removing Columns

You temporarily add or remove columns in a pane or View to get a better overview of the properties.

Afficher plus
action_close

The EcoStruxure Building Operation database is based on objects. Some objects are created when the database in installed, others are created by the engineer. Depending on the object type and your permissions, you can configure objects in a many different way.

Objects that are relevant for the user are presented in the System Tree pane and in the List View. To ease recognition of objects, every object type is represented by an icon.

Object Names

All objects in the EcoStruxure Building Operation database have to have a name. The EcoStruxure Building Operation objects are case-sensitive and differentiates between upper and lowercase characters. ​

Pour plus d'informations, voir Object Names .

Object Properties

Every object in the EcoStruxure Building Operation database has a number of different properties. Properties can be of two different types: read only and read/write. Read only properties are dimmed and cannot be changed. Read/write properties can be changed.

Pour plus d'informations, voir Object Properties .

Content Types

Content types are predefined layouts that you save to reuse for specific types of folders or container objects.

Pour plus d'informations, voir Content Types .

List View Features

You use the List View to view, manage, and mass edit objects in the EcoStruxure Building Operation database.

Pour plus d'informations, voir List View Features .

To add and remove columns
  1. In WorkStation, in the pane or View, right-click the column heading and then click Add/remove columns .

  2. In the Add/Remove dialog box, select the columns you want to add or clear the columns you want to remove.

  3. Click OK .

When you log out from WorkStation, the pane or View returns to the default columns.

  • EcoStruxure Building Operation Objects
  • Vue Liste
  • Add/Remove Columns Dialog Box (List View)