earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: WorkStation, Project Configuration Tool
功能: 基本功能, 工程
产品版本: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2018/5/18

Creating a Utility Object

You create a utility object for use during system maintenance or testing. A utility object can be created at the top level of an EcoStruxure BMS server. However, for the sake of organization it is recommended that you create the utility object inside a folder on the server.

显示更多
action_close

The EcoStruxure Building Operation software is equipped with three types of utilities: Signal Generators, Simple Math Operators, and Timed Force objects. These utilities are used for testing, for example, trend logs and alarms.

有关更多信息,请参阅 WorkStation .

Signal Generator

Signal Generator is used to create a sinusoidal, square, or saw tooth curve. Signal generator can also be used to generate a setpoint, an alarm, or an event.

Simple Math Operators

Simple Math Operator is used to add, subtract, multiply, and divide a one value from another.

Timed Force Objects

Timed Force objects are utility objects that force an override of the actual value of an analog, digital, or multistate output for a period of time specified either as a time duration or as a selected end date and time.

有关更多信息,请参阅 Timed Force Objects .

To create a utility object
  1. In WorkStation, in the System Tree pane, select the folder.

  2. In the File menu, point to New and then click Utility .

  3. In the object type list of the Create Object wizard, select the object type.

  4. In the Name box, type a name for the utility object.

  5. In the Description box, type a description and then click Create .

The utility object is created. If you created a Signal Generator or Simple Math Operator object, you next configure the object, using the Basic properties tab. If you created a Timed Force object, you next configure the object's force type as either force until or force duration, using the Basic properties tab, and then use the Parameters tab to configure other object properties as needed.

  • Utilities
  • 文件菜单 – 新建子菜单
  • Create Object Wizard – Naming the Object Page
  • Signal Generator Properties - Basic Tab
  • Simple Math Operator Properties - Basic Tab
  • Configuring a Timed Force Object for Force Until
  • Configuring a Timed Force Object for Force Duration
  • Timed Force Objects