earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: User Management
Product version: 2.0, 2.1, 3.0, 3.1
5/18/2018

Guest User Account

You create a Guest user account when you need a limited view of the system that does not require any log on.

The Guest user account is created in the Users folder of the default domain in the System Tree pane. There can only be one Guest user account. You can rename the Guest user account. The password for the Guest user account is preconfigured and cannot be changed. The password for the Guest user account never expires. You can disable the Guest user account when needed.

If the security banner is enabled the guest log on cannot be used. For more information, see Security Banner  .

You can set the policies for a user account group to log on to the Guest user account when a user account that belongs to the group is logged off. When logging off from the Guest user account, you log off to another user account. For more information, see Automatic Logoff to Guest Account .

If the EcoStruxure Building Operation software fails to auto log on using the Guest user account, no event is generated.

  • User Account Management Overview
  • User Accounts and User Account Groups
  • Guest Account Properties
  • Automatic Logoff to Guest Account
  • 1Configuring a User Account Group to Log off to the Guest User Account
  • Security Banner