earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Пользовательский интерфейс

Пользовательский интерфейс


Продукты: WorkStation, Project Configuration Tool
Функции: Базовые функции, Разработка
Версия продукта: 2024, 7.0
02.12.2024

Timed Force Multistate Object Properties – State Configuration Tab

Use the State Configuration tab to configure the state properties of the Timed Force Multistate object.

 
action_zoom_plus_stroke Timed Force Multistate object properties – State Configuration tab
Рисунок: Timed Force Multistate object properties – State Configuration tab

Таблица: State Configuration Tab

Component

Description

Number of states 

Enter the number of states to be used in this object, up to a maximum of 256 states.

State Definitions

Displays a list of the states created in the Timed Force Multistate object, along with the Label text string associated with each state.

  • Timed Force Multistate Object
  • General Information Properties – Basic Tab
  • Timed Force Multistate Object Properties – Parameters Tab
  • References Tab
  • Timed Force Multistate Object State Configuration