earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Koncept

Koncept


Produkter: AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funktionaliteter: Maskinteknik, Användarhantering
Produktversion: 3.2, 3.3, 2022
2020-10-15

Customized Navigation Workflow

Use this workflow to create a customized navigation pane in a workspace or panel.

 
action_zoom_plus_stroke Create a customized navigation pane flow chart
Figur: Create a customized navigation pane flow chart

Create a menu

Create a menu object to be used in the navigation pane.

Mer information finns i Creating a Menu .

Create a workspace or a panel

Create the workspace or panel where you want to add the navigation pane.

Mer information finns i Creating a Workspace .

Mer information finns i Creating a Panel .

Add a navigation pane to the workspace or panel with the menu as initial path

Add a navigation pane to the workspace or panel and use the menu as initial path.

Mer information finns i Adding a Component to a Workspace .

Mer information finns i Creating a Panel .

  • Customized Navigation
  • Creating a Menu
  • Creating a Workspace
  • Creating a Panel
  • Adding a Component to a Workspace