earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 工程, 用户管理
产品版本: 2023
2022/12/17

Customized Navigation Workflow

Use this workflow to create a customized navigation pane in a workspace or panel.

 
action_zoom_plus_stroke Create a customized navigation pane flow chart
图: Create a customized navigation pane flow chart

Create a menu

Create a menu object to be used in the navigation pane.

有关更多信息,请参阅 Creating a Menu .

Create a workspace or a panel

Create the workspace or panel where you want to add the navigation pane.

有关更多信息,请参阅 Creating a Workspace .

有关更多信息,请参阅 Creating a Panel .

Add a navigation pane to the workspace or panel with the menu as initial path

Add a navigation pane to the workspace or panel and use the menu as initial path.

有关更多信息,请参阅 Adding a Component to a Workspace .

有关更多信息,请参阅 Creating a Panel .

  • Customized Navigation
  • Creating a Menu
  • Creating a Workspace
  • Creating a Panel
  • Adding a Component to a Workspace