Funkcje: Inżynieria, Zarządzanie użytkownikiem
Wersja produktu: 3.2, 3.3, 2022
2020-10-15

Customized Navigation

You use the Navigation Pane to build a customized structure for navigation. The Navigation pane can be used in a workspace or a panel.

The content of a navigation pane is a referenced menu object. The objects in a navigation pane have the same context menus as they do in the System Tree pane. The navigation pane is static and only displays objects that were added to the menu object.

Navigation Pane components are not shown in WebStation in this version.

  • Workspace Customization
  • Customized Navigation Workflow
  • Workspace Customization
  • Panel Components
  • Panel Navigation
  • Adding a Component to a Workspace
  • Creating a Panel
  • Creating a Menu