earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: User Management
Product version: 2024, 7.0
12/2/2024

Guest Account Properties

Use the Guest Account Properties dialog box to view or edit the properties of the user account.

 
action_zoom_plus_stroke Guest Account Properties
Figure: Guest Account Properties

Table: Guest Account Properties

Property

Description

 
action_zoom_plus_stroke

Add

Click to add a user profile to the user account. For more information, see User Accounts and User Account Groups .

 
action_zoom_plus_stroke

Edit

Click to edit the selected user profile. For more information, see User Accounts and User Account Groups .

 
action_zoom_plus_stroke

Remove

Click to remove the selected user profile. For more information, see User Accounts and User Account Groups .

Expires on

Enter the date and time the Guest user account is to expire.

Disabled

Select True to disable the Guest user account.

System of measurement

Select the measurement system to be used when the Guest user account is logged on. For more information, see Changing the WorkStation Measurement System .

  • Guest User Account
  • User Accounts and User Account Groups
  • Changing the WorkStation Measurement System