earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 用户管理
产品版本: 2023
2022/12/17

Guest Account Properties

Use the Guest Account Properties dialog box to view or edit the properties of the user account.

 
action_zoom_plus_stroke Guest Account Properties
图: Guest Account Properties

表格: Guest Account Properties

Property

Description

 
action_zoom_plus_stroke

Add

Click to add a user profile to the user account. 有关更多信息,请参阅 User Accounts and User Account Groups .

 
action_zoom_plus_stroke

Edit

Click to edit the selected user profile. 有关更多信息,请参阅 User Accounts and User Account Groups .

 
action_zoom_plus_stroke

Remove

Click to remove the selected user profile. 有关更多信息,请参阅 User Accounts and User Account Groups .

Expires on

Enter the date and time the Guest user account is to expire.

Disabled

Select True to disable the Guest user account.

System of measurement

Select the measurement system to be used when the Guest user account is logged on. 有关更多信息,请参阅 Changing the WorkStation Measurement System .

  • Guest User Account
  • User Accounts and User Account Groups
  • Changing the WorkStation Measurement System