Funzionalità: Gestione dell'utente
Versione del prodotto: 3.2, 3.3, 2022
15/10/2020

Workspace Path, Object, and Command Customization

Software permissions limit the paths, objects, and commands that are available in a workspace. For example, a user with No Access permissions for a particular path cannot see any of the path objects displayed in the System Tree pane. A user with Read permissions for a path can see the path objects but cannot issue any commands because the objects are not made available.

Per maggior informazioni, consulta Software Permissions .

Workspaces and software permissions are linked to user account groups. User accounts inherit the workspaces and permissions of all user account groups in which the user account is a member. Per maggior informazioni, consulta Software Permissions, User Accounts, and User Account Groups .

  • Workspace Customization
  • Workspace Components and Customization
  • Software Permissions
  • Software Permissions, User Accounts, and User Account Groups