Software permissions limit the paths, objects, and commands that are available in a workspace. For example, a user with No Access permissions for a particular path cannot see any of the path objects displayed in the System Tree pane. A user with Read permissions for a path can see the path objects but cannot issue any commands because the objects are not made available.
Więcej informacji zawiera Software Permissions .
Workspaces and software permissions are linked to user account groups. User accounts inherit the workspaces and permissions of all user account groups in which the user account is a member. Więcej informacji zawiera Software Permissions, User Accounts, and User Account Groups .