earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-B, Enterprise Server, IP-IO , MP-C, MP-V, AS-P, Project Configuration Tool, RP-C
功能: 工程, 硬件
产品版本: 3.0, 3.1, 3.2
2023/1/18

SmartX IP Controller Device Memory

SmartX IP Controller devices have three types of memory:

  • Flash memory: for boot loader, operating system, application software, and configuration storage

  • RAM: for runtime operation

  • FRAM non-volatile memory: for data retention in the case of power outage

You can manually back up or restore SmartX IP Controller devices to a storage location on a PC or network. 有关更多信息,请参阅 BACnet Backup and Restore

When SmartX IP Controller devices are part of an EcoStruxure BMS, the configuration data automatically resides in the parent EcoStruxure BMS server. The EcoStruxure Building Operation database and the SmartX IP Controller device database are synchronized to help ensure there is always one backup available that can be used to restore the SmartX IP Controller device memory. Scheduled backups can provide additional protection against application and data loss. In addition, device-specific values (for example, AHU or heat pump data) are duplicated in the parent server to facilitate device replacement scenarios.

重要:

For VAV controllers, ensure you back up and save the flow balance data, as this data is not covered by the database synchronization described above.

  • SmartX IP Controller - MP Series Models
  • SmartX IP Controller - IP-IO Modules
  • SmartX IP Controller - RP Series Models
  • MP-Cs
  • MP-Vs
  • RP-Cs
  • IP-IO Modules
  • SmartX IP Controller Device Firmware Management
  • Free Object System Memory Utilization in SmartX IP Controllers
  • Application Images
  • SmartX IP Controller Communication
  • Association Selection Workflow
  • Configure an Online SmartX IP Controller Workflow
  • SmartX IP Controller Diagnostics
  • Device Discovery for SmartX IP Controller Devices
  • SmartX IP Controller Device Management
  • Automatic Time Sync for SmartX IP Controllers
  • BACnet Backup and Restore
  • Backing Up Flow Balance Data in an MP-V