Use the List View context menu to perform a number of operations on the selected object or objects.
The List View context menu is context sensitive. This means that it displays the commands available for the selected object or objects.
Command |
Description |
New |
Click to open the New submenu where you add new objects. |
Import |
Click to import an object to the EcoStruxure Building Operation database. |
Export |
Click to export an object from the EcoStruxure Building Operation database. |
Advanced |
Click to open the Advanced submenu where you select or clear content types or find out which objects that are using the selected content type. Więcej informacji zawiera List View Context Menu - Advanced Submenu . |
Cut |
Click to cut the selected object. |
Copy |
Click to copy the selected object. |
Paste |
Click to paste a cut or copied object. |
Paste as shortcut |
Click to paste the path to an object. |
Paste special |
Click to paste special. |
Duplicate |
Click to duplicate the selected object. |
Move |
Click to select a different location for the selected object. |
Delete |
Click to delete the selected objects. |
Rename |
Click to rename the selected object. |
Create shortcut |
Click to create a shortcut to the selected object. |
List View settings |
Click to open the List View settings submenu. Więcej informacji zawiera List View Context Menu - List View Settings Submenu . |