earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface de utilizador

Interface de utilizador


Produtos: AS-B, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Funcionalidades: Alarmes, Funcionalidade básica, Engenharia, Importar/exportar, Agendas, Tendências
Versão do produto: 3.2, 3.3, 2022
15-10-2020

List View Context Menu

Use the List View context menu to perform a number of operations on the selected object or objects.

Nota

The List View context menu is context sensitive. This means that it displays the commands available for the selected object or objects.

 
action_zoom_plus_stroke The commands that are always present on the List View context menu
Imagem: The commands that are always present on the List View context menu

Tabela: List View Context Menu Standard Commands

Command

Description

New

Click to open the New submenu where you add new objects.

Import

Click to import an object to the EcoStruxure Building Operation database.

Export

Click to export an object from the EcoStruxure Building Operation database.

Advanced

Click to open the Advanced submenu where you select or clear content types or find out which objects that are using the selected content type. Para mais informações, consulte List View Context Menu - Advanced Submenu .

Cut

Click to cut the selected object.

Copy

Click to copy the selected object.

Paste

Click to paste a cut or copied object.

Paste as shortcut

Click to paste the path to an object.

Paste special

Click to paste special.

Duplicate

Click to duplicate the selected object.

Move

Click to select a different location for the selected object.

Delete

Click to delete the selected objects.

Rename

Click to rename the selected object.

Create shortcut

Click to create a shortcut to the selected object.

List View settings

Click to open the List View settings submenu. Para mais informações, consulte List View Context Menu - List View Settings Submenu .

  • EcoStruxure Building Operation Objects
  • List View Features
  • List View Context Menu - Advanced Submenu
  • List View Context Menu - List View Settings Submenu