Productos AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, WorkStation
Funcionalidades: Ingeniería
Versión del producto: 2.0, 2.1, 3.0, 3.1
18/05/2018

Configuring WorkStation to run in Database Mode

You configure WorkStation to run in database mode when you want to save configuration changes to the EcoStruxure BMS server database but not send the changes to SmartX servers or other devices.

Mostrar más
action_close

In WorkStation you use database mode when you want to save configuration changes to the EcoStruxure BMS server database but not send the changes to SmartX servers or other devices.

Once you have selected to run WorkStation in database mode, the setting is saved for profile of the user account you used to log on to WorkStation. If you log on to WorkStation with the same user account but on a different computer, WorkStation opens in database mode.

Database Mode Indication and Default

When WorkStation is in database mode, there is an indication in the status bar.

By default, database mode is switched off.

When you open WorkStation from Project Configuration Tool, WorkStation always opens in database mode.

Database Mode Guidelines

When using database mode, consider the following:

  • Database mode is not recommended when working on live I/A Series MNL, NETWORK 8000, and MNB devices.

  • Run-time interactions between the EcoStruxure BMS server and BACnet devices (including the MP Series controllers) still function. For example, watch window and Graphics still display value updates and alarms are still processed from the device.

  • BACnet device commands (including those utilized in the MP Series controller) still execute. As a result, you can perform uploads and downloads in database mode.

To configure WorkStation to run in Database Mode
  1. In WorkStation, click the Tools menu.

  2. Click Database mode .

  3. Click Yes .

Database mode is indicated by a database icon in the status bar. Changes you make from now on are saved to the EcoStruxure BMS server database but not sent to any physical devices. To send the configuration changes to physical devices you have to deploy.

  • Database Mode
  • Tools Menu