earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms
Product version: 2023, 2024
12/17/2022

Custom Audible Alarm Alert Workflow

A custom audible alarm alert is an audio file that is played when an alarm is triggered.

 
action_zoom_plus_stroke Custom audible alarm alert flowchart
Figure: Custom audible alarm alert flowchart
Add an Audio File for a Custom Audible Alarm Alert

Add the custom audio file to the EcoStruxure BMS server where you want to hear the custom audible alarm alert.

For more information, see Adding an Audio File for a Custom Audible Alarm Alert .

Configure a Custom Audible Alarm Alert

Configure the alarm to play the custom audio file when the alarm is triggered or reset.

For more information, see Configuring a Custom Audible Alarm Alert .

  • Custom Audible Alarm Alerts
  • Alarm Functions
  • Adding an Audio File for a Custom Audible Alarm Alert
  • Configuring a Custom Audible Alarm Alert