earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: MP-C, MP-V
Functionalities: Hardware
Product version: 2.0, 2.1, 3.0, 3.1, 3.2
2/4/2019

MP Series Controller Communication Ports

The MP Series controller contains a combination of Ethernet, USB, and SmartX Sensor communication ports.

This combination includes the following ports:

  • Two 10/100 Ethernet ports

  • One USB host port

  • One USB device port

  • One sensor bus port

When both Ethernet ports are enabled, they function as an onboard Ethernet switch. Disabling the second Ethernet port disables the switching function. The switching function enables flexible network topologies. For more information, see SmartX IP Controller Network Topologies . The second port also provides a connection point for a laptop running the eCommission SmartX Controllers mobile application.

The two USB ports are reserved for future use.

The sensor bus port is designed for connection of SmartX Sensors. For more information, see MP Series Controller Sensor Bus .

  • Hardware Overview
  • MP-Cs
  • MP-Vs
  • MP Series Controller Sensor Bus
  • SmartX IP Controller Network Topologies