earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: MP-C
功能: 硬件
产品版本: 2023, 2024, 7.0
2024/10/7

Communication Ports on MP-C-15A, -18A, -18B, -24A, and -36A

arrow1_rotationEthernet Ports arrow1_rotationUSB Ports arrow1_rotationRS-485 Port

The MP-C provides the following combination of communication ports:

  • Two Ethernet ports

  • Two USB ports

  • One RS-485 port

This applies to the following MP-C models without “-M” in the product name:

  • MP-C-15A, MP-C-18A, MP-C-18B, MP-C-24A, and MP-C-36A

Ethernet Ports

The two Ethernet ports are labeled:

  • Ethernet 1

  • Ethernet 2

The two Ethernet ports are 10/100BASE-TX (RJ45) ports. When both Ethernet ports are enabled, they function as an onboard Ethernet switch. Disabling the second Ethernet port disables the switching function. The switching function enables flexible network topologies. 有关更多信息,请参阅 BACnet/IP Controller Network Topologies . The second port also provides a connection point for a laptop running the Commission mobile application.

有关更多信息,请参阅 Communication Port Wiring .

USB Ports

The two USB ports are of different types:

  • USB host port

  • USB device port

The USB host port is a USB 2.0 type-A port, which is rated 2.5 W. The USB host port is reserved for future use.

The USB device port is a USB 2.0 mini-B port. The USB device port is reserved for future use.

有关更多信息,请参阅 Communication Port Wiring .

RS-485 Port

The RS-485 port is labeled:

  • RS-485 Com A

The RS-485 port is rated 2 W (24 VDC).

The RS-485 port is an RJ45 port. 有关更多信息,请参阅 RJ45 Pinout for the RS-485 Port of the MP-C Controller .

The RS-485 port can be configured to use one of the following two communication protocols for different types of networks:

  • Sensor bus

  • Modbus

The sensor bus is designed for communication with SpaceLogic Sensor devices. 有关更多信息,请参阅 MP-C Sensor Bus .

The Modbus (RTU) network can be used for communication with standard Modbus devices. 有关更多信息,请参阅 MP-C Modbus .

有关更多信息,请参阅 Allocating Flexible Ports .

The RS-485 port is by default configured to use the following network communication protocol:

  • Sensor bus

有关更多信息,请参阅 Communication Port Wiring .

  • Hardware Overview
  • MP-C Communication Ports
  • MP-C Controllers
  • MP-C Sensor Bus
  • MP-C Modbus
  • BACnet/IP Controller Network Topologies
  • Allocating Flexible Ports
  • Communication Port Wiring
  • RJ45 Pinout for the RS-485 Port of the MP-C Controller