The MP-C is delivered with terminal blocks installed on the device. The MP-C uses pluggable terminal blocks, which are easy to install and remove from the device.
The only exception is the high power relay outputs on the MP-C-15A and MP-C-18A models, which use a two-position fixed terminal block due to current requirements.
Spare terminal blocks can be ordered separately using the part number SXWMPCCON1.
The wiring recommendations are provided separately. Mer information finns i Wiring .
MP-C-15A has 15 I/O points and the controller is equipped with six pluggable terminal blocks and one fixed terminal block.
Mer information finns i MP-C-15A Screw Terminals .
MP-C-18A has 18 I/O points and the controller is equipped with seven pluggable terminal blocks and one fixed terminal block.
Mer information finns i MP-C-18A Screw Terminals .
MP-C-18B has 18 I/O points and the controller is equipped with seven pluggable terminal blocks.
Mer information finns i MP-C-18B Screw Terminals .
MP-C-24A has 24 I/O points and the controller is equipped with seven pluggable terminal blocks.
Mer information finns i MP-C-24A Screw Terminals .
MP-C-36A has 36 I/O points and the controller is equipped with 10 pluggable terminal blocks.
Mer information finns i MP-C-36A Screw Terminals .