Our site will be unavailable from October 29-30 due to scheduled maintenance.
Thank you for your patience.
The MP-V is delivered with terminal blocks installed on the device. The MP-V uses pluggable terminal blocks, which are easy to install and remove from the device.
Spare terminal blocks can be ordered separately using the part number SXWMPVCON10001.
The wiring recommendations are provided separately. For more information, see Wiring .
MP-V-7A has seven I/O points and the controller is equipped with four pluggable terminal blocks.
For more information, see MP-V-7A Screw Terminals .
MP-V-9A has nine I/O points and the controller is equipped with four pluggable terminal blocks.
For more information, see MP-V-9A Screw Terminals .