You connect SmartX Sensors to an MP Series controller to provide the sensors with power and communication from the controller.
Install the SmartX Sensor and connect a Cat 5 (or higher) unshielded, straight-through wired cable with eight conductors (four twisted pairs) to one of the two RJ45 receptacles on the sensor. Use a cable with the wire size (cross-sectional area) 22 to 26 AWG (0.34 to 0.14 mm²).
For more information, see SmartX Living Space Sensor Base Installation Instructions .
For more information, see SmartX Living Space LCD Temperature Sensor Installation Instructions .
Connect the other end of the cable to the Sensor Bus port on the MP Series controller.
When an additional SmartX Sensor is needed, install the sensor and connect the other end of the cable to the unused RJ45 receptacle on the previous sensor.
When connecting SmartX Sensors to the MP Series controller sensor bus through a daisy-chain configuration, it does not matter if the incoming and outgoing cables are connected to one or the other sensor bus port on the SmartX Sensor.
Repeat step 3 to install a third and fourth SmartX Sensor, if the power constraints of the sensor bus allow this for the selected combination of cover and sensor base type.
Ensure that the two 2-position address DIP switches on each SmartX Sensor are configured to give the sensor a unique address on the sensor bus.
For more information, see SmartX Living Space Sensor Base Installation Instructions .
For more information, see SmartX Living Space LCD Temperature Sensor Installation Instructions .
For more information, see Configuring a SmartX Sensor .