earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 基本功能
产品版本: 2.0, 2.1, 3.0, 3.1
2018/10/24

Location of Backup Sets

arrow1_rotationMulti Server System arrow1_rotationStand-alone System

Backup sets are stored in different locations for stand-alone systems and multi-server systems.

Multi Server System

In a multi-server system with an Enterprise Server and one or more SmartX servers, the backup sets are stored on the computer that runs the Enterprise server. The SmartX server also store its own backup set.

In a multi-server system with an Enterprise Central and one or more attached Enterprise Servers, the backup sets for the Enterprise Central are stored on the computer running the Enterprise Central. The backup sets for the attached Enterprise Servers are stored on the computers running the Enterprise Servers.

Using WorkStation, you can copy the backup set to a location other than the EcoStruxure BMS server.

有关更多信息,请参阅 Copying a Backup Set to the Enterprise Server or Enterprise Central Local Directory .

In the Backup sets folder of the installation directory, two directories are created:

  • AS Archives : Lists separate subfolders that reflect the name of each SmartX server. Each subfolder contains the backup files for that SmartX server.

  • Local : Lists all the local backup files for the Enterprise Server and Enterprise Central.

 
action_zoom_plus_stroke Location of backup sets
图: Location of backup sets

Stand-alone System

In a stand-alone system the backup set is saved in the Smart Struxure server device. Using WorkStation, you can save the backup set to a location other than the SmartX server.

有关更多信息,请参阅 Saving a SmartX Server Backup Set to Another Location .

The SmartX server stores only one backup set at a time, so each new backup operation overwrites the previous backup set.

  • Backup Sets
  • Copying a Backup Set to the Enterprise Server or Enterprise Central Local Directory
  • Saving a SmartX Server Backup Set to Another Location