earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Pojęcie

Pojęcie


Produkty: MP-C, MP-V, RP-C, RP-V
Funkcje: Sprzęt
Wersja produktu: 2022, 2023
2023-11-22

RP and MP Controller Supported Building Standards

One of the cornerstones of the EcoStruxure BMS is support for open standards. As a result, the RP and MP controllers comply with the BACnet open standard, one of the most popular standards for buildings.

The RP and MP controllers can natively communicate with BACnet/IP or MS/TP networks. When the RP and MP controllers are part of an EcoStruxure BMS, the BACnet protocol is used for communication between the devices and their parent EcoStruxure BMS server and other BACnet devices on the network, including controllers. As native BACnet devices, the RP and MP controllers support BACnet services such as trends, schedules, and alarms, and the controllers can communicate with other BACnet devices on a BACnet/IP or MS/TP network. The RP and MP controllers conform to the BACnet Advanced Application Controller (B-AAC) device profile.

  • Hardware Overview
  • MP-C Controllers
  • MP-V Controllers
  • RP-C Controllers
  • RP-V Controllers