earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: MP-V
Functionalities: Hardware
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
12/20/2022

MP-V Damper Actuator

The MP-V has an integrated damper actuator, which allows for simplified installation of MP-V directly over the damper shaft.

The integrated damper actuator eliminates the need for separate installation, wiring, and positioning of the damper motor.

MP-V uses the same actuator mechanics as many Schneider Electric VAV controller models from Andover Continuum, TAC Vista, TAC I/A Series, and TAC I/NET product lines.

The actuator provides a Hall effect feedback signal that indicates actual movement, enabling an accurate indication of actual damper position. This provides a basis for precise position control that accepts a command from 0 to 100%.

The actuator also features a push button for manual positioning of the damper during commissioning and two stop screws for adjustment of the travel range.

  • Hardware Overview
  • MP-Vs