earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Tendencias
Versión del producto: 2.0, 2.1, 3.0, 3.1
24/10/2018

Change of Value Trend Log Properties – Meter Info Tab

Use the Meter Info tab to configure the meter function of the trend log.

 
action_zoom_plus_stroke Meter Info tab
Figura: Meter Info tab

Tabla: Meter Info Tab

Property

Description

Is meter log

Displays True if the trend log meter function is active.

Para obtener más información, consulte Función Contador .

Meter change time

Displays the time when the meter was changed.

Meter change user

Displays the name of the user account that changed the meter.

End time

Displays the time when the old meter was replaced.

End value

Displays the value the old meter had when it was replaced.

Start time

Displays the time when the new meter was installed.

Start value

Displays the value of the new meter when it was installed.

Meter constant

Displays the constant of the new meter. If the meter counts in kilo (10 3 ), the constant is 1000.

Min value

Displays the first value of the new meter after roll-over.

Max value

Displays the last value of the new meter before roll-over.

  • Change of Value Trend Logs
  • Función Contador
  • Trend Log Types
  • Configure Dialog Box – Configuration Tab
  • Trend Log Activation
  • Cuadro de diálogo Configurar - Pestaña Operación
  • Almacenamiento de entradas en el registro
  • Trend Log Does Not Start Record Due to the Start Condition
  • Missing Trend Log Records
  • Change of Value Trend Log Properties – Basic Tab
  • References Tab