earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 趋势
产品版本: 2024, 7.0
2024/12/2

Interval Trend Log Properties – Meter Info Tab

Use the Meter Info tab to configure the meter function of the trend log.

 
action_zoom_plus_stroke Meter Info tab
图: Meter Info tab

表格: Meter Info Tab

Property

Description

Is meter log

Displays True if the trend log meter function is active.

有关更多信息,请参阅 Meter Function .

Meter change time

Displays the time when the meter was changed.

Meter change user

Displays the name of the user account that changed the meter.

End time

Displays the time when the old meter was replaced.

End value

Displays the value the old meter had when it was replaced.

Start time

Displays the time when the new meter was installed.

Start value

Displays the value of the new meter when it was installed.

Meter constant

Displays the constant of the new meter. If the meter counts in kilo (10 3 ), the constant is 1000.

Min value

Displays the first value of the new meter after roll-over.

Max value

Displays the last value of the new meter before roll-over.

  • Interval Trend Logs
  • Meter Function
  • Trend Log Types
  • Configure Dialog Box – Configuration Tab
  • Interval Trend Log Delta
  • Trend Log Activation
  • Configure Dialog Box – Operation Tab
  • Log Record Storage
  • Trend Log Does Not Start Record Due to the Start Condition
  • Missing Trend Log Records
  • Interval Trend Log Properties – Basic Tab
  • References Tab