Funkcje: Trendy
Wersja produktu: 3.2, 3.3, 2022
2020-10-15

Extended Trend Log Properties – Meter Info Tab

Use the Meter Info tab to configure the meter function of the trend log.

 
action_zoom_plus_stroke Meter Info tab
Rysunek: Meter Info tab

Tabela: Meter Info Tab

Property

Description

Is meter log

Displays True if the trend log meter function is active.

Więcej informacji zawiera Meter Function .

Meter change time

Displays the time when the meter was changed.

Meter change user

Displays the name of the user account that changed the meter.

End time

Displays the time when the old meter was replaced.

End value

Displays the value the old meter had when it was replaced.

Start time

Displays the time when the new meter was installed.

Start value

Displays the value of the new meter when it was installed.

Meter constant

Displays the constant of the new meter. If the meter counts in kilo (10 3 ), the constant is 1000.

Min value

Displays the first value of the new meter after roll-over.

Max value

Displays the last value of the new meter before roll-over.

  • Extended Trend Logs
  • Meter Function
  • Configure Dialog Box – Operation Tab
  • Configure Dialog Box – Configuration Tab
  • Extended Trend Log Properties – Basic Tab
  • References Tab
  • Records Are Not Transferred to the Extended Trend Log