Productos AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Alarmas
Versión del producto: 2.0, 2.1, 3.0, 3.1
21/08/2018

Synchronizing Alarm Control Panels

You synchronize Alarm Control Panels to reuse the Alarm Control Panel on a parent EcoStruxure BMS server.

Aviso

Export Alarm Control Panel objects from the child server (Enterprise Server or Automation Server) and import them to the parent server (Enterprise Central or Enterprise Server) before you synchronize the Alarm Control Panel. During synchronization, all the Alarm Control Panel objects are erased from the child server.

To synchronize Alarm Control Panels
  1. Make sure that you have exported Alarm Control Panel objects from the child server and imported them to the parent server.

  2. In WorkStation, in the System Tree pane, expand the System folder.

  3. Select Alarm Control Panel .

  4. On the Actions menu, point to Advanced and then click Synchronize with parent server .

  5. Click Yes .

  • Alarm Control Panel Synchronization
  • User Actions
  • Lead and Shadow Relationship
  • Exporting a Solution
  • Importing a Solution
  • Import and Export of Alarm Solutions