earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 2024, 7.0
2024/12/2

Synchronizing Alarm Control Panels

You synchronize Alarm Control Panels to reuse the Alarm Control Panel on a parent EcoStruxure BMS server.

重要:

Export Alarm Control Panel objects from the child server (Enterprise Server or field server) and import them to the parent server (Enterprise Central or Enterprise Server) before you synchronize the Alarm Control Panel. During synchronization, all the Alarm Control Panel objects are erased from the child server.

To synchronize Alarm Control Panels
  1. Make sure that you have exported Alarm Control Panel objects from the child server and imported them to the parent server.

  2. In WorkStation, in the System Tree pane, expand the System folder.

  3. Select Alarm Control Panel .

  4. On the Actions menu, point to Advanced and then click Synchronize with parent server .

  5. Click Yes .

  • Alarm Control Panel Synchronization
  • User Actions
  • Lead and Shadow Relationship
  • Exporting a Solution
  • Importing a Solution
  • Import and Export of Alarm Solutions