earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 2024, 7.0
2024/12/2

Synchronizing Content Types

You synchronize content types to reuse the content types on a parent EcoStruxure BMS server.

重要:

Export content types from the child Ecostructure BMS server (such as an Enterprise Server) and import them to the parent server (like the Enterprise Central or Enterprise Server) before you synchronize them. During synchronization, all the content types are erased from the child server.

To synchronize content types
  1. Make sure that you have exported content types from the child server and imported them to the parent server.

  2. In WorkStation, in the System Tree pane, expand the System folder for the server that is to be synchronize with its parent.

  3. Select Content Types .

  4. On the Actions menu, point to Advanced and then click Synchronize with parent server .

  5. Click Yes .

  • Content Type Synchronization
  • Content Types
  • Lead and Shadow Relationship