earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: Enterprise Central, Enterprise Server, Software Administrator
功能: 工程
产品版本: 2024, 7.0
2025/7/23

Software Administrator – Enterprise Central View

Use the Enterprise Central view ​to start and stop the Enterprise Central service and configure the ports of Enterprise Central.

 
action_zoom_plus_stroke Enterprise Central view
图: Enterprise Central view

表格: Enterprise Central View

Component

Description

Status

Displays the current status of the Enterprise Central Windows service.

Start Service

Click to start Enterprise Central.

Stop Service

Click to stop Enterprise Central.

HTTP Port

Type the port number that Enterprise Central listens to when communicating through the Hypertext Transfer Protocol.

HTTPS Port

Type the port number that Enterprise Central listens to when communicating through the Hypertext Transfer Protocol Secure.

TCP Port

Type the port number that Enterprise Central listens to when communicating through the Transmitting Control Protocol.

System

Displays the system log.

Path

Displays the path to the folder where the Enterprise Central database and other objects created by Enterprise Central or users are stored.

 
action_zoom_plus_stroke

Open logs folder

Click to open the logs folder where you find logs such as the system log and the trace log.

 
action_zoom_plus_stroke

Open database folder

Open database folder

Click to open the database folder.

 
action_zoom_plus_stroke

A warning indicates that you entered a conflicting port number or that the service is stopping.

  • Starting the Enterprise Central Windows Service
  • Stopping the Enterprise Server Windows Service
  • Restarting the Enterprise Server Windows Service
  • Software Administrator
  • ​Configuring Server Port Settings