Alarm filters are used to set up the conditions for the alarms you want to be displayed in an Alarms pane or an Alarm View. You also use alarm filters to determine the conditions that have to be met before a sum alarm is triggered, an email notification is sent, a write to file notification is written, or an alarm is automatically assigned to a user.
Synchronize Alarm Control Panels to configure a lead-shadow relationship between Enterprise Central and the Enterprise Server on which the alarms reside.
Więcej informacji zawiera Synchronizing Alarm Control Panels .
On Enterprise Central, create the alarm Category 2 for the the Enterprise Server or automation server alarms you want to display on Enterprise Central.
Więcej informacji zawiera Creating a Category .
On Enterprise Central, create an alarm decoration rule to override one or several properties of aggregated alarms when the conditions of the alarm decoration rule are met. For this chosen condition, configure Category 2.
Więcej informacji zawiera Creating an Alarm Decoration Rule .
On Enterprise Central, create a filtered Alarm View that only displays the Category 2 alarms.
Więcej informacji zawiera Creating a Filtered Alarm View .