earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报, 工程
产品版本: 2.0, 2.1, 3.0, 3.1
2018/5/18

Configure Alarm Filters on Enterprise Central Workflow

Alarm filters are used to set up the conditions for the alarms you want to be displayed in an Alarms pane or an Alarm View. You also use alarm filters to determine the conditions that have to be met before a sum alarm is triggered, an email notification is sent, a write to file notification is written, or an alarm is automatically assigned to a user.

 
action_zoom_plus_stroke Custom audible alarm alert flowchart
图: Custom audible alarm alert flowchart
Synchrone Alarm Control Panels

Synchronize Alarm Control Panels to configure a lead-shadow relationship between Enterprise Central and the Enterprise Server on which the alarms reside.

有关更多信息,请参阅 Synchronizing Alarm Control Panels .

Create a Category

On Enterprise Central, create the alarm Category 2 for the the Enterprise Server or SmartX server alarms you want to display on Enterprise Central.

有关更多信息,请参阅 Creating a Category .

Create an Alarm Decoration Rule

On Enterprise Central, create an alarm decoration rule to override one or several properties of aggregated alarms when the conditions of the alarm decoration rule are met. For this chosen condition, configure Category 2.

有关更多信息,请参阅 Creating an Alarm Decoration Rule .

Create a Filtered Alarm View

On Enterprise Central, create a filtered Alarm View that only displays the Category 2 alarms.

有关更多信息,请参阅 Creating a Filtered Alarm View .

  • Alarm Filters
  • Alarm Categories
  • Alarm Decoration
  • Synchronizing Alarm Control Panels
  • Configuring the Category of an Alarm
  • Creating an Alarm Decoration Rule
  • Creating a Filtered Alarm View
  • Enterprise Central