Use the Search Results List context menu to perform a number of operations on the selected object or objects.
The Search View context menu is context sensitive. This means that it displays commands proper for the selected objects or properties. Some commands are only displayed for properties.
Command |
Description |
New |
Click to open the New submenu where you create new objects. Pour plus d'informations, voir File Menu – New Submenu . |
Open |
Click to open an object. |
Open in new tab |
Click to open the selected object in a new tab in the work area. |
Show in folder |
Click to display the object in its location in the System Tree folder structure. |
View |
Use the View menu to open a report, trend chart, trend log list, or add a value to the Watch pane. Pour plus d'informations, voir Actions Menu – View Submenu . |
Custom types |
Click to access Custom Types submenu and handle custom types. Pour plus d'informations, voir Actions Menu – Types Submenu . |
Value transfer settings... |
Click to open the Value Transfer Settings dialog box where you can configure the transfer interval for values between objects in the database. Pour plus d'informations, voir Value Transfer Settings . |
Select unit... |
Click to open the Select Unit dialog box. Pour plus d'informations, voir Select Unit Dialog Box . |
Select retain level... |
Click to open the Select Retain Level dialog box to configure the retain level to control what happens to values when different system events occurs. Pour plus d'informations, voir Retain Level . |
Refresh |
Click to cancel the latest command. |
Cut |
Click to cut the selected objects. The objects are placed on the clipboard. |
Copy |
Click to copy the selected objects. The objects are placed on the clipboard. |
Paste |
Click to paste a copied or cut object. |
Paste as shortcut |
Pastes a shortcut to a (copied) folder or object into the selected folder or EcoStruxure BMS server root. |
Paste special |
Pastes with the all external references intact. Pour plus d'informations, voir Copy, Paste, Duplicate, Move, Rename, and Delete . |
Duplicate |
Click to create a configurable number of copies of an object. Pour plus d'informations, voir Copy, Paste, Duplicate, Move, Rename, and Delete . |
Move |
Click to move an object to another location. Pour plus d'informations, voir Copy, Paste, Duplicate, Move, Rename, and Delete . |
Delete |
Click to open the Confirm delete dialog box where you delete the selected object. Pour plus d'informations, voir Confirm Delete Dialog Box . |
Rename |
Click to rename the selected object. |
Create shortcut |
Creates a new shortcut to a selected folder or object into the same folder as the target. |
Properties |
Click to open the Properties dialog box where you inspect or change properties for the selected object. Pour plus d'informations, voir General Information Properties – Basic Tab . |
Search View settings |
Click to access Add/Remove Column dialog box where you can change the colums that are displayed in the Search Results list. |