earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Hur göra

Hur göra


Produkter: WebStation
Funktionaliteter: Larm
Produktversion: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2018-05-18

Hiding an Alarm in WebStation

You hide an alarm in the Alarms pane or Alarm View to decrease the number of alarms shown in the Alarms list. All alarms, regardless of their status, can be hidden.

Visa mer
action_close

In the Alarms pane or Alarm View, you can hide alarms to decrease the number of alarms and sort out alarms from the list.

A hidden alarm is still active and changes its state as shown alarms. The only difference is that a hidden alarm that goes back to normal state is still visible in the Alarms pane, if hidden alarms are shown.

To hide an alarm in WebStation
  1. In the Alarms pane, click the alarm.

  2. In the Alarm Details dialog box, click Hide alarm .

The alarm is now hidden in the Alarms pane or Alarm View.

  • Hide and Show Alarms
  • Showing a Hidden Alarm in WebStation
  • Alarm Details Dialog Box