earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: WebStation
Funkcje: Alarmy
Wersja produktu: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2018-05-18

Showing a Hidden Alarm in WebStation

You show hidden alarms when you want display the alarms in the Alarms pane or Alarm View.

Pokaż więcej
action_close

In the Alarms pane or Alarm View, you can hide alarms to decrease the number of alarms and sort out alarms from the list.

A hidden alarm is still active and changes its state as shown alarms. The only difference is that a hidden alarm that goes back to normal state is still visible in the Alarms pane, if hidden alarms are shown.

To show a hidden alarm in WebStation
  1. In the Alarms pane, click the alarm.

  2. In the Alarm Details dialog box, click Show alarm .

The alarm is displayed in the Alarms pane or Alarm View when it is in an alarm state.

  • Hide and Show Alarms
  • Hiding an Alarm in WebStation
  • Alarm Details Dialog Box