earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: WebStation
功能: 警报
产品版本: 2024, 7.0
2024/12/3

Adding an Action Note to an Alarm in WebStation

You add an action note to an alarm to let others know what you have done to correct the problem that caused the alarm.

显示更多
action_close

An action note is a predefined note that contains information on what you have done to solve the problem that triggered the alarm.

You can add an action note to an alarm. In some cases, adding an action note to an alarm is optional. In other cases, you are required to enter an action note when you acknowledge the alarm.

You add an action note using WorkStation or WebStation. You can view an action note added to an alarm in WorkStation or WebStation.

To add an action note to an alarm in WebStation
  1. In the Alarms pane, click the alarm.

  2. In the Alarm Details dialog box, click Notes .

  3. In the Notes dialog box, click Action notes .

  4. Click Add .

  5. Select the action note.

  6. Click OK .

  7. Click Close .

The action note is added to the alarm.

  • Action Notes
  • Alarm Details Dialog Box
  • Notes Dialog Box – Action Notes Tab