earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebStation
Functionalities: User Management
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
5/18/2018

Add and Edit User Dialog Box

Use the Add and Edit User dialog box to add and edit a user in WebStation.

 
action_zoom_plus_stroke Add and Edit User dialog box
Figure: Add and Edit User dialog box

Table: Add and Edit User Dialog Box

Component

Description

User name

Type the user name.

Password

Type the user’s password. For more information, see Password Policy .

First name

Type the user’s first name.

Middle name

Type the user’s middle name.

Last name

Type the user’s last name.

Home email address

Type the users home email address.

Work email address

Type the user’s work email address.

Disable

Select True to disable the user account.

Force password change

Select True to force the user to change the password at next log on.

Expires on

Select a date when the user account expires.

Language

Select the user’s language. For more information, see Regional Settings .

Date, time and number format

Select the user’s date, time and number format. For more information, see Regional Settings .

System of measurement

Select the user’s system of measurement. For more information, see Regional Settings .

  • Regional Settings
  • Create and Administer User Accounts in WebStation
  • Password Policy