earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: WebStation
功能: 本地化
产品版本: 2024, 7.0
2024/12/3

Changing the User Theme Settings

You change the user theme settings so that it fits your screen.

显示更多
action_close

You can select several themes themes that control how WebStation is presented.

Dark Mode

You can configure WebStation to use dark mode:

  • Auto: Use the same configuration as in the web browser and operating system. If the web browser and operating system are configured to use dark mode, WebStation will be running in dark mode.

  • Enable: Enable dark mode regardless of the configuration in the web browser or operating system.

  • Disable: Disable dark mode regardless of the configuration in the web browser or operating system.

Size Mode

Size mode adjust fonts and icons to the size of your screen:

  • Auto: Adapts icons and font size to the screen size.

  • Small: Use small icons and fonts.

  • Large: Use large icons and fonts.

Accent Color

Accent Color is the color used in the top toolbar in WebStation. This color can be changed.

Accent color can only be configured on default system level.

To change the user theme settings
  1. In WebStation, on the Settings menu, click Options .

  2. Click User settings .

  3. Click Theme Settings .

  4. In the Dark Mode list, select if you want to use dark mode.

  5. In the Size Mode list, select the size of icons and fonts.

  6. Click OK .

  • Regional Settings
  • Theme Settings
  • Adding a Language in WebStation
  • Settings Menu – Workspace Tab
  • User Settings – Regional Settings Dialog Box