earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Commission, MP-V
Functionalities: Engineering, BACnet/IP devices
Product version: 2022, 2023, 2024
12/17/2021

Flow Balance Reports

The Commission mobile application provides the user with a means to generate a flow balance report that documents several values:

  • Box capacity at 1 inch H20 (249 Pa)

  • Box measured flow

  • Hood measured flow for each setpoint used during balancing

  • Actuator stroke and rotation

  • Flow balance time and date

  • Any comments

Using the Commission mobile application, you can create, append, and delete flow balance reports. Flow balance reports are stored on the Commission mobile application mobile device and can be retrieved and shared using the file and e-mail applications of that mobile device or Windows 10 laptop.

After flow balancing a VAV unit, you can use the Commission mobile application to create a new flow balance report, append an existing flow balance report with new information, view an existing flow balance report, or delete flow balance reports that are no longer needed.

Creating, Appending, Viewing, or Deleting a Flow Balance Report

After flow balancing a VAV unit, you can use the Commission mobile application to create, append, view, or delete flow balance reports.

For more information, see Managing Flow Balance Reports .

System Location of Flow Balance Reports

The flow balance report file is located in the CommissioningTool\ FlowBalanceReport folder. You can navigate to this folder, using either of two methods:

  • You can use a file navigation utility on the mobile device, for example File Explorer (Windows devices), to perform a search for the folder name.

  • You can select and copy all the contents of the Location box and then paste the text into the search box of a file navigation utility on the mobile device, for example File Explorer, and then execute the search.

Note:

Once you have located the report file, it can be exported. To do this, use the appropriate utility on your device and operating system to transfer the file to another location.

  • Flow Balancing
  • Managing Flow Balance Reports