You download an Application Image that contains a Configuration Menu to a SmartX IP controller to configure a device. Use this workflow to implement the Configuration Menu using the eCommission SmartX Controllers mobile application. Related information can be found in the section after the flowchart.
Transfer the Application Image to your mobile device or Windows 10 laptop.
For more information, see Transferring an Application Image File .
In the eCommission application, connect to the controller.
For more information, see Connecting to a Device through WiFi .
For more information, see Connecting to a Controller through Bluetooth .
Download the Application Image to the SmartX IP controller.
For more information, see Downloading an Image File to a SmartX IP Controller .
Download the Configuration Menu to the SmartX IP controller.
For more information, see Downloading a Configuration Menu to a SmartX IP Controller .
View the property values and modify them if needed.
For more information, see Modifying Device Properties from the Configuration Menu .